Legrand North & Central America Certifications
Legrand is committed to providing dependable, reliable, and efficient products recognized with certifications. Explore these certifications and related supporting materials that Legrand North and Central America offers.
Lighting & Controls
Certification | Brand | Description of Certification |
---|---|---|
ACGIH | Kenall | NOTE: This is an organization & not a listing. The American Conference of Governmental Industrial Hygienists (ACGIH) is a professional association of industrial hygienists and practitioners of related professions. One of its goals is to advance worker protection by providing timely, objective, scientific information to occupational and environmental health professionals. |
ADA | Kenall | Although ADA is not specific to lighting, it does impact fixture by creating standards for wall sconce projection space and hanging light clearance. Section 4.4 of the ADA states that ”objects projecting from walls with their leading edges between 27” and 80” above the finished floor shall protrude no more than 4” into walks, halls, corridors, passageways or aisles.” |
BAA Compliant | Kenall | The Buy American Act requires federal agencies to procure end items manufactured in the United States that are at least 65% domestic content between 2024-2028, and 75% by 2029. |
Buy American Act (BAA) | Wattsttopper | All items and materials manufactured in the United States |
Buy American Act (BAA) | Finelite | The Buy American Act is a U.S. federal law enacted in 1933 that mandates the federal government to prefer U.S.-made products in its procurement processes. The primary goal of the Act is to support American manufacturers and protect American jobs by ensuring that federal contracts for goods and services prioritize domestically produced items. |
CCEA Approved | Kenall | The City of Chicago Environmental Air (CCEA) rating ensures that the luminaire is inherently airtight. Wiring and/ or branch circuit terminations are sealed off and gasketed from the plenum air space. This listing ensures that the luminaire is sealed to limit air flow from the room side to the plenum. |
CE | Wattsttopper | The presence of the logo on commercial products indicates that the manufacturer or importer affirms the goods' conformity with European health, safety, and environmental protection standards. |
Chicago Plenum | Finelite | Chicago Plenum requires the housing to be airtight in addition to requiring all wiring to be sealed off and gasketed from the plenum air space. |
Chicago Plenum | Focal Point | Chicago Plenum requires the housing to be airtight in addition to requiring all wiring to be sealed off and gasketed from the plenum air space. |
cUL | Wattsttopper | The cUL mark applies to products intended for the Canadian market that have been tested and found to comply with the requirements of CAN/CSA 22.1-12, which is the Canadian Electrical Code issued by the Canadian Standards Association. |
Damp Rated | Finelite | Damp rated lights are designed to withstand moist environments, specifically those where condensation may build up in and around the fixture. Damp-rated lights can go both outdoors and indoors, but keep in mind that these fixtures can withstand moisture, but not direct contact with the elements. |
Damp Rated | Focal Point | A location that is normally or periodically subject to condensation of moisture in, on, or adjacent to, electrical equipment, and includes partially protected locations such as covered outdoor environments |
Declare / LBC Red List Free | Focal Point | "The Declare Label from the International Living Future Institute By facilitating and simplifying the exchange of complex ingredient information, Declare has positively changed the materials marketplace to enable the creation of buildings that support human and environmental health. |
Declare/Third Party Verified/ USGBC/WELL | Finelite | Over 90% of our portfolio has received third-party verified Red List Approved and Declared labels. Declare is a voluntary self-disclosure program designed by the International Living Future Institute (ILFI) which aims to transform the building materials industry towards healthier products through transparency. |
DLC | Wattsttopper | DLC, or Design Lights Consortium, is a program that promotes the quality, performance, and energy-efficiency of commercial lighting solutions. |
DLC | Finelite | Design Lights Consortium. A DLC listing means that a specific product has been tested to deliver superior energy efficiency. DLC-certified lighting fixtures generally offer higher lumens per watt (LPW). The higher the LPW, the more energy is converted into usable light (and the less energy is lost to heat and other inefficiencies). |
Energy Code | Wattsttopper | Learn how Legrand has simplified the process by offering recommended code compliant solutions designed with Wattstopper products. |
Energy Star | Focal Point | ENERGY STAR is a voluntary program of the U.S. Environmental Protection Agency that promotes energy efficiency in a wide range of consumer products and building systems. Our ENERGY STAR certified luminaires have been evaluated for compliance with more than 20 industry standards to ensure energy savings without compromising on light output or color quality. ENERGY STAR partners – including many state and local governments and energy utilities – often provide tax exemptions, credits and rebates for use of ENERGY STAR certified luminaires. |
FCC | Wattsttopper | When an electronic device has an FCC certificate, it means the product has been tested to comply with FCC standards and it has been approved. It simply means that it meets regulated limits for ionizing radiation. |
IC Rating | Finelite | Damp rated lights are designed to withstand moist environments, specifically those where condensation may build up in and around the fixture. Damp-rated lights can go both outdoors and indoors, but keep in mind that these fixtures can withstand moisture, |
ICNIRP | Kenall | NOTE: This is an organization & not a listing. The International Commission on Non-Ionizing Radiation Protection (ICNIRP) is an international commission specialized in non-ionizing radiation protection. The organization's activities include determining exposure limits for electromagnetic fields used by devices. |
IEC | Wattsttopper | IEC stands for International Electrotechnical Commission. IEC provides a standardized approach to testing and certification. IEC testing brings together the agreed-upon set of rules, specifications, and terminology that allow manufacturers to have their devices tested for conformity. |
IEC 62471 | Kenall | The International Electrotechnical Commission (IEC) standard 62471 provides guidance for evaluating the photobiological safety of lamps and lamp systems, including luminaries. It determines risk over a wide range of tests related to eye safety. |
IEC 62471/62778 | Kenall | The International Electrotechnical Commission (IEC) standard 62471 provides guidance for evaluating the photobiological safety of lamps and lamp systems, including luminaries. It determines risk over a wide range of tests related to eye safety. IEC 62778 brings clarification and guidance concerning the assessment of blue light hazard of all lighting products which have the main emission in the visible spectrum (380 nm to 780 nm). |
IK 10 | Finelite | IK Ratings are an international numeric classification to indicate the degrees of protection provided by enclosures for electrical equipment against external mechanical impacts. It provides a means of specifying the capacity of an enclosure to protect its contents from external impacts in accordance with IEC 62262:2002 and IEC 60068-2-75:1997.. IK10 Protected against 20 joules impact. Equivalent to impact of 5 kg mass dropped from 400 mm above impacted surface. |
ioXT & DLC NLC5 | Wattsttopper | Wattstopper products meet each of the eight ioXT principles which quantify the appropriate level of security surrounding passwords, interface security and cryptography, timely software and security updates, and vulnerability reporting needed for a specific product. |
IP 65 | Finelite | IP65 is an international standard that indicates that an electrical enclosure is dust tight and watertight against light pressure water spray. It is dust tight - no ingress of dust, and is protected from water jets from any direction. |
IP64/5/6 | Kenall | Ensures the enclosure is dust-tight and protected against splashing water (IP64), jet streams of water (IP65), or water projected in powerful jets (IP66) without any harmful effects. |
IP65 per IEC 60529 | Focal Point | A location that is normally or periodically subject to condensation of moisture in, on, or adjacent to, electrical equipment, and includes partially protected locations such as covered outdoor environments |
ISO 27001:2013 | Wattsttopper | Wattstopper is ISO:27001:2013 certified, meeting the world’s highest standard for information security management and viewed as a top certification by IT stakeholders when making buying decisions. The certificate provides a high level of confidence to customers that your products are secure by guaranteeing all software, firmware and products are protected. |
ligature resistant | Kenall | Based on standards of new construction, and also applicable to substantial renovations, select Kenall fixtures bearing this mark have been reviewed by mental health professionals for ligature-resistance and other safety criteria to earn a Patient Safety Standard Guidelines listing. |
MIL STD 461G | Kenall | Military Standards testing measurements cover both radiated and conducted electromagnetic emissions in addition to the maximum allowable amounts of emitted energy based upon both frequency length and field strength. Luminaires meeting MIL STD 461G pose the lowest possible likelihood of causing EMI-related issues. |
NFPA101 | Kenall | The National Fire Protection Agency (NFPA) life safety code pertains to egress facilities. The code establishes minimum criteria for the design of egress facilities so as to allow prompt escape of occupants from buildings or, where desireable, into safe areas within buildings. |
NSF | Focal Point | An NSF2 Listing denotes that the luminaire has been evaluated for corrosion resistance, cleanability and the ability of exposed material to withstand normal wear. This supports the infection control standards established by healthcare facilities as it indicates that the luminaire is easy to sanitize. |
NSF P442 | Kenall | This protocol is a series of minimum requirements for the design, construction, performance, and certifications of luminaires for cleanrooms. It requires ingress protection IEC 60529/60598 (IP-65) and NSF-2 Food Equipment certifications and a performance test for pressure decay resistance in which the sealed fixture is stressed with positive and negative pressure and checked to ensure that no leaks are present. |
NSF P495 | Kenall | A new standard of cleanliness that validates the disinfection of surfaces via narrow spectrum visible light (400 nm - 420 nm) in a controlled environment. The P495 certification demonstrates a statistically significant reduction of Staphylococcus Aureus and/or Clostridium Difficile endospores on clinically relevant surfaces, such as stainless steel and laminate. Luminaires must also be NSF-2 compliant. |
NSF2 | Kenall | An NSF2 Listing denotes that the luminaire has been evaluated for corrosion resistance, cleanability and the ability of exposed material to withstand normal wear. This supports the infection control standards established by healthcare facilities as it indicates that the luminaire is easy to sanitize. |
NYS OMH listed | Kenall | The New York State Office of Mental Health (NYS OMH) publishes patient safety standards guidelines that provides a selection of materials, fixtures, and hardware reviewed by OMH. The guidelines further their goal of reducing the risk of harm to individuals while in inpatient setting. |
OSHPD | Kenall | This listing pertains to standards that protruding objects and horizontal projections must meet in order to comply with the requirements of California Office of State Health Planning (OSHPD), California Building Code, Sections 1003.3.1 through 1003.3.4, for buildings and structures used for medical, surgical, psychiatric, nursing or custodial care for persons who are nonambulatory or bedridden. |
RoHS | Wattsttopper | The RoHS Directive and Lighting Equipment. The RoHS Directive contains exemptions allowing mercury and certain applications of lead in lighting. All other hazardous substances may not exceed the MCV as a percentage by weight per homogenous material (please see RoHS Directive exemptions for more details. |
Title 24 JA8 | Finelite | "Title 24 is the sixth section of the California Energy Code that states that all residential and non-residential buildings must only use a capped number of watts per linear foot of luminaires to reduce energy consumption. Our products are highly efficient and can be tailored to your exact light output requirements to help you achieve project goals. An Addendum to the California Energy Code - JA8 is a subsection of Title 24 that lists specific requirements a light source must meet to qualify as residential lighting. This includes points like CRI > 90, CCT < 4000k, R9 > 50, and 6 other categories. We’re proud to say that our products have qualified under these standards." |
Title 24 JA8 | Focal Point | "California’s Building Energy Efficiency Standard Title 24, Part 6 is designed to ensure new and existing residential and nonresidential buildings achieve energy efficiency. Considered one of the strictest energy codes in the United States, it is published and regularly updated by the California Energy Commission (CEC) to preserve the quality of the environment through the reduction of energy usage by limiting the allowed lighting power, in watts, in a building. Residential luminaires must be certified to meet the High Efficacy Lighting standards under Joint Appendix 8 (JA8). Our 2016 & 2019 JA8 High Efficacy Lighting luminaires meet the strict energy standards and other criteria specified by the CEC for both residential and nonresidential applications, ensuring energy savings without compromising on light quality." |
UL | Wattsttopper | UL Certification means the product or service meets local and federal environmental and safety regulations. The UL Mark signals to consumers that the manufacturer follows standards for quality and safety. |
UL, cUL | Focal Point | UL Certification means the product or service meets local and federal environmental and safety regulations. The UL Mark signals to consumers that the manufacturer follows standards for quality and safety. |
UL/ETL | Kenall | The UL symbol signifies that Underwriter's Laboratory (UL) has determined that a manufacurer has demonstrated the ability to produce a product complying with UL's requirements with respect to specific risk, performance under specific conditions, compliance with regulatory codes and specified standards, or any other conditions as determined by UL. A product bearing the ETL Mark is determined to have met the minimum requirements of the applicable product safety standards as certified by Interek, a Nationally Recognized Testing Laboratory (NRTL). The “US” next to the mark indicates compliance with US standards, and “C” next to the mark indicates compliance with Canadian standards. |
UL48 | Kenall | The ANSI/UL 48 signifies that a manufacturer’s products are in compliance with Underwriter’s Laboratories (UL) requirements for all electric signs, art forms and outline lighting for use in accordance with the National Electrical Code, NFPA 70 |
UL924 | Kenall | ANSI/UL 924 is UL’s Standard for Safety of Emergency Lighting and Power Equipment. ANSI/UL 924 listed electrical exit signs are tested and given a visibility rating of at least 100 feet, requiring them to be legible from a 100 foot viewing distance in total darkness. The battery backup is tested and must provide at least 90 minutes of emergency operation. Letters must be red or green and at least 6” height with a 3/4” letter stroke. |
Wet Location Rated | Focal Point | A location in which water or other liquid can drip, splash, or flow on or against electrical equipment. Focal Point wet location luminaires are tested to be suitable for use in wet location rated indoor or covered outdoor environments. |
Lighting & Controls Certification Supporting Resources
Shading
Certification | Brand | Description of Certification |
---|---|---|
CE | Wattsttopper | The presence of the logo on commercial products indicates that the manufacturer or importer affirms the goods' conformity with European health, safety, and environmental protection standards. |
cUL | Wattsttopper | The cUL mark applies to products intended for the Canadian market that have been tested and found to comply with the requirements of CAN/CSA 22.1-12, which is the Canadian Electrical Code issued by the Canadian Standards Association. |
DLC | Wattsttopper | DLC, or Design Lights Consortium, is a program that promotes the quality, performance, and energy-efficiency of commercial lighting solutions. |
Energy Code | Wattsttopper | Learn how Legrand has simplified the process by offering recommended code compliant solutions designed with Wattstopper products. |
FCC | Wattsttopper | When an electronic device has an FCC certificate, it means the product has been tested to comply with FCC standards and it has been approved. It simply means that it meets regulated limits for ionizing radiation. |
IEC | Wattsttopper | IEC stands for International Electrotechnical Commission. IEC provides a standardized approach to testing and certification. IEC testing brings together the agreed-upon set of rules, specifications, and terminology that allow manufacturers to have their devices tested for conformity. |
RoHS | Wattsttopper | The RoHS Directive and Lighting Equipment. The RoHS Directive contains exemptions allowing mercury and certain applications of lead in lighting. All other hazardous substances may not exceed the MCV as a percentage by weight per homogenous material (please see RoHS Directive exemptions for more details. |
UL | Wattsttopper | UL Certification means the product or service meets local and federal environmental and safety regulations. The UL Mark signals to consumers that the manufacturer follows standards for quality and safety. |
Shading Certification Supporting Resources
Critical Power and Infrastructure
Certification | Brand | Description of Certification |
---|---|---|
ETL verified to TIA 568C.2 Category 6a and Category 6 component performance standards | Ortronics and Quiktron | "UMJ605 A Category 6 UMJ style jack that meets TIA component performance requirements and is ETL Verified to TIA 568-C.2 Cat 6 standards. It has a dielectric withstand of 1000 VAC RMS, AC 60Hz or 1414 VDC and a DC current rating of 1.5A per conductor at 20°C ambient. KMJ Jacks Meets TIA 568-C.2 Cat 6 requirements, is compliant with Power over Ethernet (PoE) requirements, and is backward compatible with Cat 3, 5, and 5e. It has an insulation resistance of 500MΩ minimum and a dielectric withstand of 1000 VAC RMS, AC 60Hz or 1414 VDC P-P. " |
IEC 27001:2013 | KVM | This certification covers the protection and security of the software and firmware developed by Legrand for connected devices, embedded systems, and IT systems in the DPC R&D centers in Somerset, NJ, Reno, NV, Canonsburg, PA and Zwickau, Germany, including the brands Raritan, Server Technology, and Starline. ISO/IEC 27001:2013 is an information security standard published by the International Organization for Standardization (ISO), the world’s largest developer of voluntary international standards, and the International Electrotechnical Commission (IEC). |
IP54 and NEMA 3R rating | Starline | "NEMA 3R Protects against rain, sleet, snow, and ice, and quickly disperses water through a small drain IP54 Protects against dust and water ingress from all sides" |
ISO 27001:2013 | KVM | " The company announces the achievement of ISO/IEC 27001:2013 certification for its Data, Power & Control division (DPC), having earned the highest standard for managing information security in its products and services. In addition to achieving all 114 process controls required for ISO27001 certification in its engineering group, Legrand adheres to NIST and ISO standards (including ISO 9001 and ISO 14001) as well as incorporates additional vulnerability and penetration testing for its network-connectable products. This additional testing puts products through additional cybersecurity testing to uncover areas of vulnerability or risk of unauthorized access to fix problems before they arise in real-world applications." |
Low Smoke, Zero Halogen [LSZH] cable type | Ortronics and Quiktron | The material is a thermoplastic, low smoke zero halogen (LSZH) flame retardant, UV stabilized, natural jacketing compound with excellent extrusion properties. Its composition includes Carbon, Hydrogen, Oxygen, Silicon, and Calcium. |
MSA Compliant | Approved Networks | A multi-source agreement (MSA) is an agreement among multiple manufacturers to make products which are compatible across vendors, acting as de facto standards, establishing a competitive market for interoperable products. Products that adhere to multi-source agreements (MSAs) include: optical transceivers, fiber optic cables; and other networking devices. MSAs strictly define the operating characteristics of these network devices so that system vendors may implement ports in their devices (e.g. Ethernet switches and routers) that allow MSA compliant devices produced by name brands, as well as third party vendors, to function properly. |
UL & UL 1863 | Ortronics and Quiktron | Underwriters Laboratories (UL) is a safety science company that evaluates products for electrical safety and design quality. Products with UL listing adhere to UL's standards for electrical safety, structural integrity, and design soundness. |
UL 94V-0, plastic housing & UL 1863 | Ortronics and Quiktron | "UL 94 V-0 Vertical Burn: Burning stops within 10 seconds, and no flaming drips are allowed. UL 94 V-1 Vertical Burn: Burning stops within 60 seconds, and no flaming drips are allowed. UL 94 V-2 Vertical Burn: Burning stops within 60 seconds, and flaming drips are allowed. If you’ve come across products with a UL 1863 Listing, it means the product is deemed safe for use. Essentially, you don't need to worry about exposed wires or electrical shock, even in challenging environments." |
UL, ETL listed, and CE marked | Starline | "Underwriters Laboratories (UL) is a safety science company that evaluates products for electrical safety and design quality. Products with UL listing adhere to UL's standards for electrical safety, structural integrity, and design soundness. Electrical Testing Laboratories (ETL) is a certification mark used by Intertek, a company specializing in testing, inspection, and certification. Products with ETL listing meet North American safety standards for gas-fired appliances and electrical equipment. European Conformity (CE) is a certification mark indicating that a product complies with European standards. CE certification is mandatory for certain products to be sold within the European Economic Area (EEA)." |
Critical Power & Infrastructure Certification Supporting Resources
Electrical Wiring Systems
Certification | Brand | Description of Certification |
---|---|---|
cULu | Wiremold | Product(s) evaluated and found to be in compliance with applicable UL and CSA product safety standards and listed by UL Solutions. |
cTUVRheinlandus | Wiremold | TUV Rheinland is an OSHA certified NRTL (Nationally Recognized Test Lab). Products evaluated, tested and certified by TUV Rheinland that comply with the UL and CSA standards would bear the cTUV Rheinlandus mark |
UL | Connectrac | Product(s) evaluated and found to be in compliance with applicable UL and CSA product safety standards and listed by UL Solutions. |
UL | Pass & Seymour | Evaluated and found to be in compliance with applicable UL and CSA product safety standards and listed by UL Solutions. Products Include: Receptacles, GFCIs, USBs, Plugs and Connectors to the description of certification. |