text.skipToContent text.skipToNavigation

Wattstopper® FDP-300 Series DALI Digital Sensors Now Available

Enabling connected outdoor lighting systems for smarter, more energy efficient, and data-driven applications


San Jose, Calif., March 14, 2019– Legrand, North & Central America and its Eliot program introduced new capabilities for OEMs with the availability of the Wattstopper FDP-301SR sensor. The sensor features a streamlined design for fixture integration and enables bi-directional communication between the sensor and connected driver or wireless node. This is the first sensor from Legrand to bring occupancy detection to a connected outdoor fixture.

The FDP-301SR sensor is ideal for parking facilities, gas stations, pedestrian street lighting, and warehouses. It is compatible with many intelligent drivers including the Philips Lighting SR® platform, and when connected, the sensor does not need its own power supply reducing cost and saving space inside the luminaire.

For design engineers, the sensor addresses two critical market needs: a way to add advanced SR functionality to existing luminaries and the ability to offer end-users an easy hardware upgrade without opening the luminaire.

Other features and benefits include:

  • Maximum sequence of operations and two dedicated lens options that provide reliable coverage from 20 to 40-foot mounting heights
  • Design flexibility as sensors provide two different methods to attach to a luminaire * Ease of installation and setup through local or remote commissioning via Legrand Sensor Configuration app
  • IP66 and IK08 rated to ensure the highest protection against water, dust, and other non-corrosive material as well as against external mechanical impacts
  • Code compliance with latest ASHRAE 90.1/ IECC and California Title 24 outdoor lighting control requirements

 “Using these sensors in an outdoor lighting solution empowers facility engineers and city managers in the simple monitoring, control, commissioning, and troubleshooting of outdoor lighting while also maximizing safety and security,” said Kathleen Neighbors, Wattstopper Product Manager at Legrand. “Outdoor lighting systems are experiencing a shift from analog to digital, network-controlled solutions. The FDP-301SR assists with this transition in a way that truly enables intelligent lighting solutions while also ensuring the substantial energy and maintenance cost savings the Wattstopper product line is known for.”


###

AboutWattstopper

Wattstopper, a product line of Legrand, offers the most comprehensive line of simple, scalable, and flexible energy-efficient lighting controls and solutions for commercial and residential applications. The Wattstopper range of products, programs, and services has been helping customers save energy, meet green initiatives, and comply with energy codes for more than 30 years. legrand.us/Wattstopper

About Legrand and Legrand, North and Central America

Legrand is a global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial, and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value is a prime vector for growth, including, in particular, connected devices stemming from Legrand’s global Eliot (Electricity and IoT) program. Legrand reported sales of $6.2 billion (USD) in 2017. Legrand has a strong presence in North and Central America, with a portfolio of well-known market brands and product lines that includes AFCO Systems, C2G, Cablofil, Chief, Da-Lite, Electrorack, Finelite, Luxul, Middle Atlantic Products, Milestone AV, Nuvo, OCL, On-Q, Ortronics, Pass & Seymour, Pinnacle, Projecta, QMotion, Quiktron, Raritan, Sanus, Server Technology, Solarfective, Vaddio, Vantage, Wattstopper, and Wiremold. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating, and DJSI (ISIN code FR0010307819) www.legrand.us.

 
###

Media Contact:
Mary Placido
, Legrand Building Control Systems
415-218-3627 mary.placido@legrand.us