Safety Recall: Legrand Under Cabinet Power and Lighting (4 outlet power strip), Model PX1001
Purchased between February 2011 and August 2012
Legrand Wiremold has determined that the hot and neutral wires are reversed on the receptacles which could pose a potential risk of electric shock. Consumers should immediately stop using the power strips and return them to Legrand Wiremold for a replacement or refund. The Model PX1001 power strips, which retailed at $39.99, came in red packaging. The manufactured dates, presented as product date codes January 2011 through June 2012, are found imprinted on a circle on the bottom with an arrow pointing to the number of the month and the year in the center, “11” or “12”.
To determine if your Legrand PX1001 power strip is subject to this voluntary recall, call Legrand Wiremold toll free at: 800-621-0049 between 8 a.m. to 5 p.m. EST Monday through Friday.