text.skipToContent text.skipToNavigation

Consulting-Specifying Engineer Magazine Readers Award Wattstopper® with Two Product of the Year Awards

The Wireless Receptacle Controls (WRC) Series and FSP-201 Outdoor Sensor received the 2016 GOLD Award and SILVER Award in the Lighting Controls category



San Jose, Califronia
September 15, 2016


 

Legrand, North America announced today that two of its Wattstopper® products, the Wireless Receptacle Controls (WRC) Series and FSP-201 Outdoor Sensor received the 2016 GOLD Award and SILVER Award in the Lighting Controls category, as voted by Consulting Specifying Engineer readers in its annual Product of the Year contest. These two Wattstopper products exemplify the breadth of its code-compliant, cost-effective and proven indoor and outdoor lighting controls.

“We want to thank the more than 309,000 engineers in the commercial buildings and facilities marketplace who cast their votes,” said Jim Young, Vice President of Marketing, Building Controls Systems division at Legrand. “Wattstopper has a valued legacy of delivering control solutions that are energy-efficient, easy to install and use, ensure maximum flexibility, and that meet the ever-evolving code requirements of our industry.”

The Gold Award-winning WRC Series leverages lighting control sensors for improved ROI. Designed to be the easiest, lowest cost retrofit solution for plug load controls, it brings huge energy and cost savings potential in integrating lighting and plug load control. Available in two versions, the WRC Series offers more options to meet desired project goals.

The Silver Award was given to the FSP-201, which mounts in an outdoor lighting fixture to provide multi-level control based on motion and/or daylight contribution. Part of the award-winning FSP-200 Series product line, the FSP-201 provides an expanded choice of operating voltages from 12 to 32 VDC. It is IP66 rated (when mounted within a fixture), simplifies compliance with ASHRAE 90.1/IECC (2012) and California Title 24 (2013) garage and outdoor lighting requirements, and using the Wattstopper handheld wireless configuration tool (FSIR-100) simplifies ladder-free configuration.


About Wattstopper

Wattstopper, a product line of Legrand, offers the most comprehensive line of simple, scalable and flexible energy efficient lighting controls and solutions for commercial and residential applications. The Wattstopper range of products, programs, and services have been helping customers save energy, meet green initiatives and comply with energy codes for more than 30 years. www.legrand.us/wattstopper.


About Legrand

Legrand is the global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value is a prime vector for growth, including in particular connectable products enhancing value in use. Legrand reported sales of $5.3 billion in 2015. Legrand has a strong presence in North America, with a portfolio of well-known product lines that include C2G, Cablofil, Electrorack, Middle Atlantic, Nuvo, On-Q, Ortronics, Pass & Seymour, QMotion, Quiktron, Raritan, Vantage, Wattstopper, and Wiremold. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating and DJSI
(ISIN code FR0010307819). www.legrand.us.

###


Media Contact:

Mary Placido, Wattstopper PR
(415) 218-3627 pr@wattstopper.com