text.skipToContent text.skipToNavigation

Legrand Features Nuvo P4300, Multi-Zone Flagship Player for Player Portfolio Music System, at CEDIA 2017

Features Line’s First Backlit Touch Screen Display and Delivers Highest Quality Audio to Three Zones Simultaneously with 100 Watts of Power


San Diego
September 7, 2017
 

​​​​​​​Legrand, the global specialist in electrical and digital building infrastructures, showcases its Nuvo P4300 Player, the new flagship rack mount model of its Player Portfolio line at CEDIA 2017. The model is the first in the line to have a backlit touch screen and features its most powerful three amplifier design, enabling three different audio programs to be played simultaneously.

The P4300 allow users to get even more enjoyment from their favorite music via  popular streaming services, including Spotify, iHeartRadio, TuneIn, Napster, Deezer and SiriusXM, as well as from content stored on networked computers and iOS and Android portable devices. The system consistently delivers the highest quality audio with 100 watts of power via its efficient Class D amplifiers. The P4300 also incorporates powerful DSP for every zone to allow for the tailoring of speakers.

The music is controlled and directed via the model’s backlit touch screen display that shows system status and zone names. The display also provides system configuration information that aids in installation.

“The P4300 represents an important stage in the evolution of the Player Portfolio line, and only increases the appeal of professionally-installed whole home audio systems,” said Desirée Webster, Legrand’s senior marketing communications manager, Electrical Wiring Systems. “The multi-zone capabilities and backlit touch screen offer unprecedented power, flexibility, convenience and ease-of-use so your favorite music is always at hand.”

Super efficient Class D amplifiers provide enhanced audio and power output, which remains consistent when set to 4, 6 or 8 ohms within the app during setup. All line inputs and line outputs use a combination 3.5mm analog/Toslink connection. It has side-mounted heat sinks and no fans to allow convenient single-space rack mounting.

The Nuvo P4300 is currently available for MSRP $2,299.00.

About Legrand and Legrand, North & Central America

Legrand is a global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value is a prime vector for growth, including, in particular, connected devices stemming from Legrand’s global Eliot (Electricity and IoT) program. Legrand reported sales of $5.6 billion in 2016. Legrand has a strong presence in North and Central America, with a portfolio of well-known product lines that include C2G, Cablofil, Electrorack, Luxul, Middle Atlantic, Nuvo, OCL, On-Q, Ortronics, Pass & Seymour, Pinnacle, QMotion, Quiktron, Raritan, Solarfective, Vantage, Wattstopper, and Wiremold. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating and DJSI (ISIN code FR0010307819) www.legrand.us

#  #  #

 

Media Contacts:

Feintuch Communications

Doug Wright / Richard Roher                                                 

212-808-4903 / 212-808-4902

legrand@feintuchpr.com