WattStopper brings time-saving ladder-free sensor configuration to warehouses
SANTA CLARA, Calif., June 26, 2014 – WattStopper has introduced time-saving remote functionality to warehouse lighting control with a game-changing new high/low bay sensor. The sensor is packed with features to simplify installation and maintenance, making it easier to manage energy effectively in applications where lighting is mounted as high as 40 feet.
Part of a new family of fixture-mounted sensors, the infrared (IR) remote-controlled occupancy sensor includes a pre-installed lens for mounting heights from 15 to 40 feet. For aisle way applications, installers can snap on a rotatable masking ring, included with the PIR (passive infrared) sensor. This new lens design simplifies ordering and installation compared to previous products that either work only at specific heights, or require on site assembly using specific lenses for different applications.
The compact sensor also features accessible onboard controls for installers who prefer presetting special control parameters. A companion product includes the same controls and lens, but without the IR capability.
WattStopper launched ladder-free sensor configuration with its Digital Lighting Management controls, and subsequently added remote capability to parking lot sensor and now to high bay sensors. Installers and facility managers can store multiple sensor parameter profiles in a single IR remote control device to speed configuration and optimize control for different applications.
WattStopper (www.wattstopper.com) a Legrand group brand, is a leading manufacturer of energy efficient lighting controls for commercial and residential use. We help customers find convenient ways to save energy, meet green initiatives, and comply with energy codes with our comprehensive range of products, programs, and services. Legrand (www.legrand.com), located in Limoges, France, is the world specialist in products and systems for electrical installations and information networks, offering solutions for use in residential, commercial and industrial buildings.
Editorial Contact and Photos:
Evelyne McCleland
WattStopper | 2800 De La Cruz Blvd. Santa Clara, CA 95050
E-mail:pr@wattstopper.com