Cablofil Universal Drop Out provides tray support and smooth transitions for fiber cables
New dropout solution designed for high-capacity data centers
Mascoutah, Ill. — August 17, 2017 — The Cablofil Universal "Hang On" Drop Out (UDO), available now from Legrand, is a first-of-its-kind cable dropout solution for high-capacity data centers that protects the integrity of trays and cables to help optimize performance.
The UDO does not require any cutting or modifications to the existing wire mesh tray and features a 120-degree bend to ensure cables do not have any potential pinch points or kinks. This will benefit data centers that are challenged with managing the expansive lengths of heavy overhead cabling necessary to meet consumer demand for faster data download, streaming and transfer speeds.
Data centers are also increasingly using fiber-optic cables. If fiber is bent at too sharp of an angle, performance can be hampered or the cables can even break. The smooth bend of the UDO is optimal for fiber optic, and the product also supports copper and Power over Ethernet (PoE) cabling.
“Trends like cloud computing, online video and mobile technology have led to higher capacity data centers that are fitting more cables into their spaces,” said Bob Crain, director of marketing and product development for the Cablofil product line at Legrand. “Trays are full and data centers are looking for a new way to drop cables without compromising performance. The Universal "Hang On" Drop Out is the ideal solution.”
The UDO is also easy to install — it snaps onto the edge of an existing tray. The ease of installation makes moves, adds and changes easier to accomplish.
“Unlike competitive products, you don’t have to thread the cables or cut the tray, so it’s easy to get cable in and out of the UDO itself,” Crain said. “If the server room is rearranged and cabinets are moved, a person can physically pick up the UDO and move it. This ability to quickly reconfigure is critical in ever-changing data centers.”
The UDO is available in four sizes: 8, 12, 18 and 24 inches. It comes in a variety of finishes, including electrozinc, white, black or a customer color to match a data center. Hardware is included to bolt down the UDO if desired, and there are tie-down slots for cables that are sized for hook-and-loop fasteners.
For more information on the Universal "Hang On" Drop Out, visit www.legrand.us/cablofil.
###
About Legrand and Legrand, North & Central America
Legrand is a global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value is a prime vector for growth, including, in particular, connected devices stemming from Legrand’s global Eliot (Electricity and IoT) program.
Legrand reported sales of $5.6 billion in 2016. Legrand has a strong presence in North and Central America, with a portfolio of well-known product lines that include C2G, Cablofil, Electrorack, Luxul, Middle Atlantic, Nuvo, OCL, On-Q, Ortronics, Pass & Seymour, Pinnacle, QMotion, Quiktron, Raritan, Solarfective, Vantage, Wattstopper, and Wiremold. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating and DJSI (ISIN code FR0010307819) www.legrand.us.
Media Contact:
Keely Coppess, Public Relations Manager
Two Rivers Marketing
(515) 557-2025, KeelyC@2rm.com