The need to reliably dim an LED without flickering and jarring adjustments is as important as ever. As of August 2023, incandescent light bulbs can no longer be found on store shelves, yet dimming technology has long been engineered to adapt to these types of light bulbs. However, LED light bulbs can use 75% less energy and last roughly 25% longer than incandescent light bulbs. With the growing need for energy efficiency in the home and adherence to local energy codes, LED lighting is not just the way of the future, it's the way of lighting today.
Replace any Switch with a Dimmer
Easily replace any existing basic single-pole or 3-way switch or dimmer in less than 15 minutes. With no neutral wire required, the radiant® LED Advanced Dimmer works in both new construction and retrofit applications and works with LED dimmable bulbs.
Save Energy.
Set the Ambiance.
Upgrade Your Home Design.
Dim any Dimmable LED with Legrand
LED Dimmers work with virtually any bulb and décor style.
Dimmer switches feature clean lines for a sophisticated touch.
Designer dimmer switches seamlessly add style and functionality.